Technical FAQs

Ask a Question

What is the minimum load and maximum rating for the NW M2C/M6C Programmable Contacts?

Minimum Load = 100 mA/24 V
Breaking Capacity at a
Power Factor (p.f.) of 0.7
240 Vac 5 A
380 Vac 3 A
24 Vdc 1.8 A
48 Vdc 1.5 A
125 Vdc 0.4 A
250 Vdc 0.15 A


CTA-ID : 8904
Was this helpful?
What can we do to improve the information ?