Technical FAQs

Ask a Question

Why could the snubbers on the Omegapak 8804 braking unit explode?

If the GTO on the Draking module is shorted this would happen. Recommend that also check the braking resistor.


CTA-ID : 4135
Was this helpful?
What can we do to improve the information ?