Technical FAQs

Ask a Question

Does the Omegapak 8804 PF01 pneumatic sensor option take a 3-15 psi signal and convert it to a 4-20 ma output for the drive?

No, the PF01 works more like a speed pot. You supply a 10V reference, and it converts the 3-15 psi to a 0-10V output, for a speed reference to the drive. He will need to contact a Square D distributor or Field Office to see if the part is available.


CTA-ID : 4157
Was this helpful?
What can we do to improve the information ?