Technical FAQs

Ask a Question

What are the repair parts for the H324A, series F5? (may be shown as F05)

Issue:
The list of repair parts is needed for Safety Switch catalog number H324A, series F5.

Product Line:
Heavy Duty Safety Switch

Environment:
Applicable only to H324A, Series F5

Cause:
The repair parts numbers for the H324A, series F5, are shown in the below list. These are the parts that can be replaced. Other parts are not replaceable.

Resolution:
The replacement parts for the H324A, series F5 (F05) are as follows. No other parts (enclosure, labels) are available.
-Complete Line Base - 4056703350 - (requires one line base per switch - includes phynolic base, arc suppressors, lugs, rotor, switching blades, and fuse clips if applicable)
-Line Base mounting screws - 4020546401 (requires 6 per line base)
-Load Base Assembly - 4056678250 (requires one per phase - includes phynolic base, lugs and fuse clips)
-Load Base mounting screws - 4020546401 (requires 2 per load base)
-Arc Suppressor Assembly - 4053922001(requires one per phase)
-Arc Suppressor mounting screw - 4020514501
-Lug Assembly - CL20F (incl. 6 lugs - requires mounting screws below)
-Lug Assembly mounting screw - 2140122240 (per lug)
-Switch Mechanism - 4056678650 (also requires Interlock Shaft Gasket 4056786001)
-Switch Mechanism mounting screws- 2299940562 (requires 2)
-Handle Assembly - 4056663550 (requires handle gasket 4056603101)
-Lockplate - 4056672101
-Lockplate mounting screws - 2299940562 (requires 2)
-Cover latch and spring - one each of 4056607201 (latch) and 4022304301 (spring)
Was this helpful?
What can we do to improve the information ?