Technical FAQs

Ask a Question

What wire-binding torque should be applied to the AL100FA lug for the FA, FH, FI and FAL, FHL, FIL breakers?

Cu #14 - #1/0 (2.5-50 mm^2) Strand: 80 lb-in.
Al #12 - #1/0 (2.5-50 mm^2) Strand: 80 lb-in.
Al #12 - #10 (2.5-6 mm^2) Solid: 40 lb-in.
Cu #14 - #10 (2.5-6 mm^2) Solid: 80 lb-in.


CTA-ID : 8660
Was this helpful?
What can we do to improve the information ?