Technical FAQs

Ask a Question

Which wire sizes are approved for the AL50FA lug for the FA, FI, and FH breakers?

#14-#10 AWG Sol (2.5-6 mm2) Cu
#14-#4 AWG Str (2.5-25 mm2) Cu
#12-#10 AWG Sol (2.5-6 mm2) Al
#12-#4 AWG Str (2.5-25 mm2) Al


CTA-ID : 6415
Was this helpful?
What can we do to improve the information ?