Technical FAQs

Ask a Question

Does Altivar ATV66 have a bumpless transfer feature when going from a 4-20mA signal to keypad mode?

No, you can not do a bumpless transfer from a 4-20mA signal to keypad mode because when going to keypad mode you are changing it to 3-wire control which requires that the start button be pushed..


CTA-ID : 7050
Was this helpful?
What can we do to improve the information ?