Technical FAQs

Ask a Question

What is the % ( percentage ) of Altivar ATV66 parts made in the USA and the % of parts made elsewhere?

There is not way to tell the percentages because different part manufacturers are used. However the unit is assembled in the USA and has the ``Made in the USA`` label on it.


CTA-ID : 7060
Was this helpful?
What can we do to improve the information ?