Technical FAQs

Ask a Question

What is the MTBF hours for the Altivar ATV66?

MTBF for drive controllers 1 - 100 HP (sizes 1-5) is 65,000 hours. For drive controllers 125 - 400 HP (sizes 6-7), the MTBF is 30,000 hours.


CTA-ID : 7041
Was this helpful?
What can we do to improve the information ?