Technical FAQs

Ask a Question

Can a board be added to allow for a 4-20ma signal input for speed control on the Omegapak 8804?

Part number 8804 MC12 is for the isolated option board kit. 52011-889-50 is an isolation module: DC to DC signal converter/isolator which allows for what customer desires.


CTA-ID : 4143
Was this helpful?
What can we do to improve the information ?