Technical FAQs

Ask a Question

Do part number 52011-003-50 ( gate driver cards ) have to be ordered as a pair for the Omegapak 8804?

There are two of these per phase, if one fails there is a strong possibilty that the other one could have been damaged thus they are sold as pairs only.

CTA-ID : 4107
Was this helpful?
What can we do to improve the information ?