Technical FAQs

Ask a Question

Can the Omegapak 8804 be adjusted above 60 hz?

Yes, Need to remove snip out resistor R251 on the main control board for 90 hz operation, then adjust the speed


CTA-ID : 4121
Was this helpful?
What can we do to improve the information ?