Technical FAQs

Ask a Question

What is the part number of the Omegapak 8804 DOI ( digital operator interface ) keypad?

The DOI keypad part number is 52011-850-50 and it is important to verify the revision letter of keypad being replaced because there are compatibility issues if don`t match up properly between keypad, DOI board and serial board..


CTA-ID : 4099
Was this helpful?
What can we do to improve the information ?