Technical FAQs

Ask a Question

What are the repair parts for the H221NRB, series F1? (may be shown as F01)

The repair parts for the H221NRB, series F1(F01) are as follows. No other parts are available.

Line Base Assembly -40566-422-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-410-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Handle Gasket - 40566-031-01
Lockplate - 40566-376-01
Neutral Assembly - SN03
Neutral Bonding Screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)
Line & load base mounting screw - 40205-160-01 (3 required for line & 2 required for load base)
Arc suppressor mounting screw - 40205-145-01 (1-required)
Lockplate mounting screw - 22999-405-62 (2 required)


CTA-ID : 8107
Was this helpful?
What can we do to improve the information ?