Technical FAQs

Ask a Question

What is the part number for the load base assembly for a H365, Series E2 safety switch?

The load base assembly is 40552-190-50SEL. This is for one phase only. You may also need to consider replacing the phase insulator 40552-191-01.


CTA-ID : 1681
Was this helpful?
What can we do to improve the information ?