Technical FAQs

Ask a Question

What wire-binding torque should be applied to the the AL50FA lug for the FA, FI, and FH breakers?

#14-#10 AWG Sol (2.5-6 mm2) Cu; 35 lb-in (4 N-m)
#14-#4 AWG Str (2.5-25 mm2) Cu; 35 lb-in (4 N-m)
#12-#10 AWG Sol (2.5-6 mm2) Al; 15 lb-in (2 N-m)
#12-#4 AWG Str (2.5-25 mm2) Al; 35 lb-in (4 N-M)


CTA-ID : 6419
Was this helpful?
What can we do to improve the information ?