Technical FAQs

Ask a Question

What is the required torque for the CU100FA lug for the FA, FH, FC, and FI breakers?

#14-#10 AWG Str/Sol (2.5-6 mm2) Cu; 35 lb-in (4 N-m)
#8 AWG Str/Sol (10 mm2) Cu; 40 lb-in (5 N-m)
#6-#4 AWG Str (16-25 mm2) Cu; 45 lb-in (5 N-m)
#3-#1 AWG Str (35-50 mm2) Cu; 50 lb-in (6 N-m)


CTA-ID : 6439
Was this helpful?
What can we do to improve the information ?