Technical FAQs

Ask a Question

What wire-binding torque should be applied to the CU30FA4 lug for the FC, FCP, and FCL breakers?

35 lb-in (4 N-m)


CTA-ID : 6425
Was this helpful?
What can we do to improve the information ?