Technical FAQs

Ask a Question

Which wire sizes area approved for the CU100FA lug for the FA, FH, and FI breakers?

#14-#10 AWG Str/Sol (2.5-6 mm2) Cu
#8 AWG Str/Sol (10 mm2) Cu
#6-#4 AWG Str (16-25 mm2) Cu
#3-#1 AWG Str (35-50 mm2) Cu


CTA-ID : 6421
Was this helpful?
What can we do to improve the information ?