Technical FAQs

Ask a Question

Can you use a Class 8430 relay on the output of the Altivar ATV66 drive?

No, this relay have a pre-set line voltage it expects to see at all time. The varying voltage due to the drive would cause it to not function properly.

CTA-ID : 7011
Was this helpful?
What can we do to improve the information ?