Technical FAQs

Ask a Question

Is there a problem with having a full voltage starter in front of the Altivar ATV66 drive?

Would want the starter to close before the drive gets the run command. Also would want to wait to open the starter until the motor is stopped by the drive unless he wants to freewheel all the time.

CTA-ID : 6991
Was this helpful?
What can we do to improve the information ?