Technical FAQs

Ask a Question

Is there a video available that explains how to program the Altivar ATV66 drive.

The video is available on the AC Drives and Softstarts CD Rom, part number 8800EP9801, and the video number is8803AV9801. If this is not available through literature fulfillment 1-800-888-2448, then try to order through a distributor.

CTA-ID : 6985
Was this helpful?
What can we do to improve the information ?