Technical FAQs

Ask a Question

What is the purpose of the Connected/Closed Switch (EF) switch?

This switch combines the device-connected and device-closed information
to produce circuit-closed information. The connected/closed switch (EF) is
supplied as an option and must be used with an additional auxiliary switch
(OF) and fits into its connector (it is not available for ring terminals).


CTA-ID : 8830
Was this helpful?
What can we do to improve the information ?