Technical FAQs

Ask a Question

Could you confirm the mounting torque for the bolts attaching the side plates 32532 to the mounting base 32514 for the NS630?<br />

The adaptation manual indicates 62 lb.-in. (7 Nm) and a M5*35 screw. However, use common sense and do not exceed what is reasonable for material. France has been asked to review.


CTA-ID : 8896
Was this helpful?
What can we do to improve the information ?