Technical FAQs

Ask a Question

What is the wire range or terminal lug data for the H326N and is there an alternate lug for larger wires?

Issue:
Terminal lug data or wire range of switch

Product Line:
Heavy Duty Safety Switches

Environment:
Main lug wire range

Cause:
Installation

Resolution:
The lugs on the H326N will accept (2) #3/0AWG - 500kcmil (AL/CU). There are NO Alternate lugs that allow larger wire sizes due to UL and NEC wire bending space.


CTA-ID : 1379
Was this helpful?
What can we do to improve the information ?