Technical FAQs

Ask a Question

H365R 400A 3P Heavy Duty Safety Switch is this a top hinge or side hinge - Customer must have a side hinge cover

H365R has a top hinge cover. An electrically equivalent Type 12 switch, H365AWK, is a side hinged switch and is also rated for an outdoor, Type 3R application. Removal of the drain screw from the bottom endwall is required for the Type 3R application.


CTA-ID : 635
Was this helpful?
What can we do to improve the information ?