Technical FAQs

Ask a Question

Will the Altivar ATV66 accept a 2-10 VDC analog signal?

No, the drive is setup to accept a 0-10 volt or 4-20mA signals to operate between low speed and high speed.


CTA-ID : 6923
Was this helpful?
What can we do to improve the information ?