Technical FAQs

Ask a Question

Why does the speed potentiometer adjust speed in hand and auto for this 8804 Omegapak?

With the E07 option card, if terminal 16 is tied to 78 the drive will use the POT for speed in hand and auto.
Remove this jumper to allow a separate auto speed signal.

CTA-ID : 4043
Was this helpful?
What can we do to improve the information ?