Technical FAQs

Ask a Question

What is the maximum current of Aux. switch for QOU breaker?

Max current of auxiliary switch for QOU breaker is 5A at 120VAC, 50/60Hz.


CTA-ID : 8889
Was this helpful?
What can we do to improve the information ?