Technical FAQs

Ask a Question

What are the ratings of the Powerpact P and R frame OF, SD, and SDE contacts?

Switch Electrical Characteristics
Contacts Standard Low-level
Rated current 6 A 5 A
Minimum load 10 mA at 24 V 1 mA at 4 V


CTA-ID : 8875
Was this helpful?
What can we do to improve the information ?