Technical FAQs

Ask a Question

What are the repair parts for a DU325 Series E03 General Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40510-467-51
Arc supressor - 40510-574-02
Lug assembly - 40251-136-50
Base assembly mounting screws - 21427-202-41 (6) required for line base & (7) required for load base.
Arc supressor mounting screw - 40205-082-01
Lug mounting nut - 23427-028-00



CTA-ID : 8344
Was this helpful?
What can we do to improve the information ?