Technical FAQs

Ask a Question

What are the repair parts for a DU324RB Series E02 or E03 General Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Line base assembly - 40510-595-50 (Note: if line base or Rotor is needed order both)
Arc shield - 40510-540-01
Lug assembly - 40251-052-50
Rotor - 40510-556-50 (Note: if line base or Rotor is needed order both)
Base assembly mounting screws - 40205-065-01 (4) required for line base
Arc shield mounting screw - 40205-082-01


CTA-ID : 8331
Was this helpful?
What can we do to improve the information ?