Technical FAQs

Ask a Question

What is recommended specification for motors to be used with AC drives?

The spec is Nema MG-1, Part 31.

The standard can be obtained by purchase from
There is some helpful information in the Application Guide for AC Adjustable Speed Drive Systems available at as a free download.

CTA-ID : 7084
Was this helpful?
What can we do to improve the information ?