Technical FAQs

Ask a Question

Where is the Shield connection for Analog Inputs on the Altivar ATV58 located?

The control terminal strip contains two pull-apart terminal blocks. The S terminal , Shield connection , is located to the right of the two pull-apart terminal blocks. It is one of the mounting screws for the main control board. It is chassis ground. It is important for the drive to be properly grounded according to the installation guide.


CTA-ID : 6888
Was this helpful?
What can we do to improve the information ?