Technical FAQs

Ask a Question

Can one potentiometer be used to operate three Altivar ATV66 drives at slightly different speeds if needed.

Told him to wire the pot to +10, com & AI1 on first drive, tie the commons and then parallel the wiper to each drives AI1 terminal. Then go to each drives low and high speed setting to scale the speed ranges.




CTA-ID : 6866
Was this helpful?
What can we do to improve the information ?