Technical FAQs

Ask a Question

Does the Altivar 58 unit have Auto-Manual switching?

Yes, the unit does have Auto/Manual switching.
The function is used to switch between two different analog input signals for the speed reference.
The parameter is rFc in the I-O menu. The exact function varies if there is an option card.
See the programming guide for additional information.

CTA-ID : 6852
Was this helpful?
What can we do to improve the information ?