Technical FAQs

Ask a Question

What is the maximum number of aux. switches OF that can be installed on a Powerpact P-Frame or R Frame breaker?

An R-frame, P-frame or NS630b-NS3200 circuit breaker can accommodate up to three 1A/1B auxiliary switches.

CTA-ID : 8873
Was this helpful?
What can we do to improve the information ?