Technical FAQs

Ask a Question

Has a UL 489 M9 through-door operator. Does it interlock with the door?

Yes, it interlocks with the door.


CTA-ID : 8854
Was this helpful?
What can we do to improve the information ?