Technical FAQs

Ask a Question

What are the different Cradle Position Switches, and how do they operate?<br /><br />

Three series of optional auxiliary switches are available for the cradle:
CE indicates the connected position.
CD indicates the disconnected position. This position is indicated when the required clearance for isolation of the power and auxiliary circuits is reached.
CT indicates the test position. In this position, the power circuits are disconnected and the auxiliary circuits are connected.


CTA-ID : 8844
Was this helpful?
What can we do to improve the information ?