Technical FAQs

Ask a Question

How is a DRK30 Class R Fuse Kit assembled to the General Duty switch fuse clips?

Product Feature

Product Line:
GD SS Accessory


The DRK30 adapters barbed end is pushed firmly into a slot in the base near the LINE SIDE fuse clips. The circular portion of the adapter should engage the slot in the fuse clip. The adapter should not be able to be removed once properly installed. Three adapters are included in each kit.

CTA-ID : 1592
Was this helpful?
What can we do to improve the information ?