Technical FAQs

Ask a Question

What is accuracy of the ATV18 speed control?

Issue: What is accuracy of the ATV18 speed control?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: With Slip Compensation on, +/- 1% of nominal speed for torque variation of 0.2TN ( Nominal torque ) to TN. With drive auto tuned is +/- 0.5% of nominal speed for torque variation of 0.2TN to TN


 
Was this helpful?
What can we do to improve the information ?