Technical FAQs

Ask a Question

What do you need to do when starting up the Altivar ATV56 drive and get a NRP on display?

Told him that on this unit he must place a jumper wire from +24 to logic input 1. Informed that NRP stands for no run permissive. LI1 has to always be high when in any mode for unit to operate and has to have 24v on it consequently.


CTA-ID : 6700
Was this helpful?
What can we do to improve the information ?