Technical FAQs

Ask a Question

Can the ATV18 be used on corner or center tapped delta distriburtion system?

Issue:  Can the ATV18 be used on corner or center tapped delta distriburtion system?
 
Product Line:  ATV18
 
Environment:  All
 
Cause:  N/A
 
Resolution:  Yes, they can. The only concern would be that if the drive sees fault current, the ground current may be high enough to damage the filter board.


 
Was this helpful?
What can we do to improve the information ?