Technical FAQs

Ask a Question

Is it a problem to run the Altivar ATV18 drive at 2 hz most of the time?

At low frequencies, the motor cannot cool itself and may burn. Recommend using Gear Reducers as well as contacting the motor manufacturer to see if low speed operation is ok.


CTA-ID : 4386
Was this helpful?
What can we do to improve the information ?