Technical FAQs

Ask a Question

Can the Altivar ATV18 freewheel stop?

Issue: Can the Altivar ATV18 freewheel stop?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: Yes, in level 2 paramters disable the bra function which stands for brake ramp adaptation.


 
Was this helpful?
What can we do to improve the information ?