Technical FAQs

Ask a Question

What are the repair parts for a D326NTR Series E01 General Duty Safety Switch?

Issue:
Repair parts

Product Line:
GD Safety Switch

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The parts listed here are the only field replaceable parts.
Line base assembly - 40510-482-51
Load base assembly - 40510-484-51
Arc supressor - 40510-574-02
Lug assembly - 8011612250
Neutral assembly - D600SN
Base assembly mounting screws - 21427-202-41 (6) required for line base & (7) required for load base.
Arc supressor mounting screw - 40205-082-01
Lug mounting nut - 23427-028-00
Neutral assembly mounting screw - 40205-065-01 (4) required
Neutral bonding assembly - 40283-312-50
Cross Arm Insulator - 40510-308-01 (insulator) and 40510-318-01 (dust shield - retainer for insulator)



CTA-ID : 8350
Was this helpful?
What can we do to improve the information ?