Technical FAQs

Ask a Question

Are EDB circuit breakers available with a 50 degree C calibration?

Yes. Add suffix CA to the catalog number.


CTA-ID : 2549
Was this helpful?
What can we do to improve the information ?