Technical FAQs

Ask a Question

Is the Altivar ATV18 drive UL and CE listed?

Issue: Is the Altivar ATV18 drive UL and  CE  listed?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: The unit is CE and UL listed.


 
Was this helpful?
What can we do to improve the information ?