Technical FAQs

Ask a Question

Is the keypad included as standard with the ATV58 type H drive?

No. The keypad must be ordered separately. The keypad part number is VW3A58101U.
There is no way to alter the ATV58H part number so that they keypad is included.

CTA-ID : 6804
Was this helpful?
What can we do to improve the information ?