Technical FAQs

Ask a Question

Can the Altivar ATV56 internal power supply be wired to power a transducer.

As long as the LI inputs total and transducer power required doesn`t exceed 210ma but need to remember if have an external short it could damage the internal supply. So, while it may be used we do not recommend this.

CTA-ID : 6773
Was this helpful?
What can we do to improve the information ?